:DISPlay:GRAPh:Y:STOP
Flex Apps:
FlexPLL
Command Syntax
:DISPlay:GRAPh:Y:STOP <amplitude>
<amplitude> is a double.
Query Syntax
:DISPlay:GRAPh:Y:STOP?
Description
For FlexPLL's graph of the Jitter Transfer Function, sets the stop (maximum) amplitude for the graph's Y-axis in dB. To set the Y-axis start (minimum) amplitude, use the :DISPlay:GRAPh:Y:STARt command.
Example Command Sequence
:DISPlay:GRAPh:X:CENTer 10E6; :DISPlay:GRAPh:X:SPAN 20E6; :DISPlay:GRAPh:Y:STARt -5.00E1; :DISPlay:GRAPh:Y:STOP 1.00E1;