:DISPlay:VRESponse
Flex Apps:
FlexPLL
Command Syntax
:DISPlay:VRESponse {RESPonse{1} | RMEMory{1:4}}
Query Syntax
:DISPlay:VRESponse?
Query Response
{RESP1 | RMEM1 | RMEM2 | RMEM3 | RMEM4}
Description
Selects to display the measurement results table for the selected response or response memory. When selected, any displayed measurement annotation is moved to the selected plot. Using this command has no affect on the return of measurement values as the response or memory selection is accomplished in the individual measurement queries as described in the :MEASure subsytem.