:SYSTem:FACTory
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:SYSTem:FACTory
Description
Sets FlexPLL to its factory preset settings. Use the *OPC? query to notify the calling program when an operation is complete. Factory preset is the combination of the default settings and additional settings. There is no query form of this command or ability to undo its action.
Use of an *OPC? query to pause program execution while waiting for this command to execute.
| Feature | Setting |
|---|---|
| SCPI Server Setup | |
| GPIB | Enabled |
| VXI-11 | Enabled |
| USB | Enabled |
| Telnet | Disabled |
| Sockets | Enabled |
| USB | Enabled |
| Jitter Source Connection Setup Dialog Settings | |
| Connection Method | LAN |
| LAN Server | VXI-11 |
| Host Name / IP Address | HostName |
| VXI-11 Device Index | 0 |
| DCA Connection Setup Dialog Settings | |
| Connection Method | LAN |
| LAN Server | HiSLIP |
| FlexDCA Host Name | HostName |
| HiSLIP1 Device Index | 0 |
| HiSLIP1 Port | 4880 |