:SYSTem:GTLocal

Flex Apps:
FlexDCA
FlexRT
FlexPLL

Command Syntax

:SYSTem:GTLocal

Description

Places FlexPLL in local mode which allows operation via the front panel. This is useful if you need the user to perform a front-panel task. The next command that is sent to the instrument returns it to remote mode. When ending a program, you should always issue this command to return control to the front panel.