:SYSTem:PRESets
Command Syntax
:SYSTem:PRESets <preset name>
<preset name> is a string.
Description
Loads a previously saved System Setup preset which imports the settings listed in the table below. FlexPLL comes with several PICe presets as shown in the Supplied FlexPLL System Setup Presets table in this topic. You select one of these presets to automatically configure FlexPLL with the correct settings to use during the calibration step. After the calibration, you load another preset to configure FlexPLL's settings during measurements. Presets are simple XML files so you can view their contents with a text editor. The preset configures the following modules with your saved preset settings:
- N1060A
- N107x-series Clock Recovery DCA-M
To query which presets are available for loading, use the :SYSTem:PRESets:SELections? child query.
| Dialog Settings | ||
|---|---|---|
| Source Tab | Receiver Tab | Acquisition Tab |
| System Clock Rate | Symbol Rate | Start Frequency |
| Wave Type | Auto Loop Select | Stop Frequency |
| Clock Rate | Type 2 Loop | Points / Decade |
| Pattern | Averaging | |
| Symbol Rate | ||
| Amplitude P-P (single ended) | ||
| Offset | ||
| Jitter Amplitude P-P | ||
| Output Coupling | ||
System Setup Presets
- PCIe Gen1 (81150A-60A Cal)
- PCIe Gen1 (81150A-60A Meas)
- PCIe Gen1 (M8000 Cal)
- PCIe Gen1 (M8000 Meas)
- PCIe Gen2 (81150A-60A Cal)
- PCIe Gen2 (81150A-60A Meas)
- PCIe Gen2 (M8000 Cal)
- PCIe Gen2 (M8000 Meas)
- PCIe Gen3 (81150A-60A Cal)
- PCIe Gen3 (81150A-60A Meas)
- PCIe Gen3 (M8000 Cal)
- PCIe Gen3 (M8000 Meas)
- PCIe Gen4 (81150A-60A Cal)
- PCIe Gen4 (81150A-60A Meas)
- PCIe Gen4 (M8000 Cal)
- PCIe Gen4 (M8000 Meas)
- PCIe Gen5 (81150A-60A Cal)
- PCIe Gen5 (81150A-60A Meas)
- PCIe Gen5 (M8000 Cal)
- PCIe Gen5 (M8000 Meas)
- PCIe Gen6 (81150A-60A Cal)
- PCIe Gen6 (81150A-60A Meas)
- PCIe Gen6 (M8000 Cal)
- PCIe Gen6 (M8000 Meas)
Presets can only be saved from the Receiver Setup dialog. There is no programming command for this task.
For FlexPLL application, requires revision A.06.70 and above.