:SYSTem:SOFTware:LICenses:FEATure?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:SYSTem:SOFTware:LICenses:FEATure? "<license>"
Where <license> is the identification string representing a package license or legacy feature license.
Query Response
String identifying feature. For example, "EnhancedJitterAnalysis".
Description
This command takes a Query Argument from the following tables and returns the associated Descriptive Name that is also listed in the following tables. The arguments identify either a licensed package or a legacy feature. Be sure to enclose the parameter with quote characters. Entering an other parameter (or no parameter) results in an –224, Illegal parameter value message.
| Query Argument | Returned Description Name | Description |
|---|---|---|
| L-MFG | N1010200A | Manufacturing Package |
| L-RND | N1010100A | Research and Development Package |
| L-SNT | N1010300A | Signal Integrity Package |
| Query Argument | Returned Description Name | Description |
|---|---|---|
| 200 | EnhancedJitterAnalysis | Enhanced Jitter Analysis |
| 201 | AdvancedWaveformAnalysis | Advanced Waveform Analysis |
| 202 | AdvancedTDRAnalysis | Enhanced Impedance and S-Parameters |
| 300 | AmplitudeAnalysis | Advanced Amplitude Analysis/RIN/Q-Factor |
| 401 | 401AdvancedEye | Advanced Eye Analysis |
| 500 | ProductivityPackage | Productivity Package |
| AFR | DCA_Automatic_Fixture_Removal | Automatic Fixture Removal in TDR Mode |
| CA4 | CAUI-4_IEEE_DCA_Application | IEEE 802.3bm-2015 CAUI-4 Measurements |
| CEI | OIF_CEI_Compliance_Application | OIF CEI Compliance Application |
| CES | OIF_CEI_Compliance_App_Switch | OIF CEI Compliance Switch Control |
| DCA | DCA_HostedOperation | Support for all DCA-X mainframe SW options, hosted mode |
| EYE | FlexEye | FlexEye Independent Eye Acquisition and Analysis |
| HST | SFF-8431_Host_Meas_Suite | SFF-8431 Host Measurement Suite |
| IE1 | IEEE_802_3_10G-KR_40G-KR4 | IEEE 802.3ap/ba, Clauses 72,84 |
| IE2 | IEEE_802_3_XLAUI_CAUI_nPPI | IEEE 802.3ba, Clauses 83A,83B,86A |
| IE3 | IEEE_802_3_40G-CR4_100G-CR10 | IEEE 802.3ba, Clause 85 |
| IE4 | IEEE_802_3_100G-KR4_100G-CR4 | IEEE 802.3bj, Clauses 92,93 |
| IES | IEEE_802_3_100G-KR4_CR4_Switch | IEEE 802.3 Compliance Switch Control |
| MOD | SFF-8431_Module_Meas_Suite | SFF-8431 Module Measurement Suite |
| MYC | DCA_UserDefinedApplication | User Defined Application |
| MYS | DCA_UserDefinedApp_Switch | User Defined Application Switch Control |
| PAM | PAM_N_Analysis | PAM-N Analysis Software |
| PM1 | PAM-4_IEEE_DCA_Application | IEEE 802.3bs Draft PAM4 Measurements |
| PM2 | N1091BSCA | IEEE 802.3bs/cd Measurement Application |
| PM2U | N1091BSUA | IEEE 802.3bs/cd Measurement Application, N1085A Upgrade |
| PM4 | PAM-4_OIF-CEI_DCA_Application | OIF-CEI 56G Draft PAM4 Measurements |
| PM5 | N109256CA | OIF-CEI-56G-VSR/MR/LR Measurement Application |
| PM5U | N109256UA | OIF-CEI-56G-VSR/MR/LR Measurement Application, N1085A Upgrade |
| PMS | PAM-4_DCA_Switch_Option | IEEE 802.3 Compliance Switch Control |
| SFS | SFF-8431_Meas_Suite_Switch | SFF-8431 Measurement Suite Switch Control |
| SIM | InfiniiSim-DCA | InfiniiSim-DCA Waveform Transformation Toolset |
| TDQ | TDECQ | TDECQ Transmitter and Dispersion Eye Closure for PAM4 |
Example Query
:SYSTem:SOFTware:LICenses:FEATure? "EYE"