:SYSTem:SOFTware:FEATures:ENABled?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:SYSTem:SOFTware:FEATures:ENABled? "<software feature>"
Where <software feature> is the identification string representing a feature that is included as part of a Manufacturing , Research and Development , or Signal Integrity package license.
Query Response
{1 | 0}
Description
Returns 1 (true) if the specified feature is enabled for use and 0 (false) if the feature is not enabled. The following table lists the valid software feature parameters for this query. These are the same strings returned by the *OPT? common command. Be sure to enclose the parameter with quote characters. Entering an other parameter (or no parameter) results in an –224, Illegal parameter value message. To return the version of an enabled software feature, use the :SYSTem:SOFTware:FEATures:VERSion? command.
| Query Argument | Software Feature |
|---|---|
| F-AEYE | Advanced Eye Analysis |
| F-AFR | Automatic Fixture Removal in TDR Mode |
| F-ATDR | Enhanced Impedance and S-Parameters |
| F-AWG | Keysight Arbitrary Waveform Generator Control |
| F-EQ | Equalizers (CTLE, DFE, LFE) |
| F-FEYE | FlexEye Independent Eye Acquisition and Analysis |
| F-FLEX | FlexDCA Remote Access Software |
| F-JIT | Enhanced Jitter Analysis |
| F-PAM | PAM-N Analysis Software |
| F-PTDQ | Partial TDECQ, Noise Margin, and SER Measurements |
| F-SIM | InfiniiSim-DCA Waveform Transformation Toolset |
| F-RRX | Provides a reference receiver Waveform Signal Processing operator that allows joint FFE/DFE optimization |
| F-TDEC | NRZ TDEC Measurement |
| F-TDQ | TDECQ Measurement and Equalizer |
| F-UDI | Unrestricted Data File Import |
| F-UDMO | User Defined Measurements and Operators |
Example Query
:SYSTem:SOFTware:FEATures:ENABled? "F-AWG"