:SYSTem:SOFTware:LICenses:INSTalled?
Query Syntax
:SYSTem:SOFTware:LICenses:INSTalled? "<package/legacy license>"
Where <package/legacy license> is the identification string representing a package license or a legacy feature license.
Query Response
Boolean, 1 or 0
Description
Returns 1 (true) if the specified package or legacy license is installed and 0 (false) if the license is not enabled. Always send the :SYST:SOFT:LIC:REFResh command before sending the :SYST:SOFT:LIC:BORRow query.
The following tables list the valid package and legacy license arguments for this query. These parameter strings are identical to those returned by the *OPT? common command. Be sure to enclose the parameter with quote characters. Entering an other parameter (or no parameter) results in an –224, Illegal parameter value message. To return the version of an installed package license, use the :SYSTem:SOFTware:LICenses:VERSion? command.
| Query Argument | Returned Description Name | Description |
|---|---|---|
| L-MFG | N1010200A | Manufacturing Package |
| L-RND | N1010100A | Research and Development Package |
| L-SNT | N1010300A | Signal Integrity Package |
| Query Argument | Returned Description Name | Description |
|---|---|---|
| 200 | EnhancedJitterAnalysis | Enhanced Jitter Analysis |
| 201 | AdvancedWaveformAnalysis | Advanced Waveform Analysis |
| 202 | AdvancedTDRAnalysis | Enhanced Impedance and S-Parameters |
| 300 | AmplitudeAnalysis | Advanced Amplitude Analysis/RIN/Q-Factor |
| 401 | 401AdvancedEye | Advanced Eye Analysis |
| 500 | ProductivityPackage | Productivity Package |
| AFR | DCA_Automatic_Fixture_Removal | Automatic Fixture Removal in TDR Mode |
| CA4 | CAUI-4_IEEE_DCA_Application | IEEE 802.3bm-2015 CAUI-4 Measurements |
| CEI | OIF_CEI_Compliance_Application | OIF CEI Compliance Application |
| CES | OIF_CEI_Compliance_App_Switch | OIF CEI Compliance Switch Control |
| DCA | DCA_HostedOperation | Support for all DCA-X mainframe SW options, hosted mode |
| EYE | FlexEye | FlexEye Independent Eye Acquisition and Analysis |
| HST | SFF-8431_Host_Meas_Suite | SFF-8431 Host Measurement Suite |
| IE1 | IEEE_802_3_10G-KR_40G-KR4 | IEEE 802.3ap/ba, Clauses 72,84 |
| IE2 | IEEE_802_3_XLAUI_CAUI_nPPI | IEEE 802.3ba, Clauses 83A,83B,86A |
| IE3 | IEEE_802_3_40G-CR4_100G-CR10 | IEEE 802.3ba, Clause 85 |
| IE4 | IEEE_802_3_100G-KR4_100G-CR4 | IEEE 802.3bj, Clauses 92,93 |
| IES | IEEE_802_3_100G-KR4_CR4_Switch | IEEE 802.3 Compliance Switch Control |
| MOD | SFF-8431_Module_Meas_Suite | SFF-8431 Module Measurement Suite |
| MYC | DCA_UserDefinedApplication | User Defined Application |
| MYS | DCA_UserDefinedApp_Switch | User Defined Application Switch Control |
| PAM | PAM_N_Analysis | PAM-N Analysis Software |
| PM1 | PAM-4_IEEE_DCA_Application | IEEE 802.3bs Draft PAM4 Measurements |
| PM2 | N1091BSCA | IEEE 802.3bs/cd Measurement Application |
| PM2U | N1091BSUA | IEEE 802.3bs/cd Measurement Application, N1085A Upgrade |
| PM4 | PAM-4_OIF-CEI_DCA_Application | OIF-CEI 56G Draft PAM4 Measurements |
| PM5 | N109256CA | OIF-CEI-56G-VSR/MR/LR Measurement Application |
| PM5U | N109256UA | OIF-CEI-56G-VSR/MR/LR Measurement Application, N1085A Upgrade |
| PMS | PAM-4_DCA_Switch_Option | IEEE 802.3 Compliance Switch Control |
| SFS | SFF-8431_Meas_Suite_Switch | SFF-8431 Measurement Suite Switch Control |
| SIM | InfiniiSim-DCA | InfiniiSim-DCA Waveform Transformation Toolset |
| TDQ | TDECQ | TDECQ Transmitter and Dispersion Eye Closure for PAM4 |
Example Command Sequence
The status variable will contain either a 1 for success or a 0 for failure.
FlexDCA.write(':SYSTem:SOFTware:LICenses:REFResh')
status= FlexDCA.write(':SYSTem:SOFTware:LICenses:BORRow? "L-RND", 5')
FlexDCA.write(':SYSTem:SOFTware:LICenses:REFResh')
status = FlexDCA.write(':SYSTem:SOFTware:LICenses:INSTalled? "L-RND"')