:SYSTem:SOFTware:LICenses:VERSion?
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:SYSTem:SOFTware:LICenses:VERSion? "<package license>"
Where <package license> is the identification string representing a package license.
Query Response
Boolean, 1 or 0
Description
Returns the version date of an installed package license in the form of "1.000". Before sending this command, always confirm that the package license is installed using the :SYSTem:SOFTware:LICenses:INSTalled? command. The following table lists the valid package license parameters for this query. These are the same strings returned by the *OPT? common command. Notice that valid parameters start with the "L-" characters. Be sure to enclose the parameter with quote characters. Entering an other parameter (or no parameter) results in an –224, Illegal parameter value message.
| Query Argument | Returned Description Name | Description |
|---|---|---|
| L-MFG | N1010200A | Manufacturing Package |
| L-RND | N1010100A | Research and Development Package |
| L-SNT | N1010300A | Signal Integrity Package |
Example Query
:SYSTem:SOFTware:LICenses:INSTalled? "L-RND"