Peaking Frequency
Flex Apps:
FlexPLL
Peaking Frequency measures frequency at the maximum peaking on the JTF response for a DUT that uses a 2nd Order PLL. The following figure shows a simplified JTF response with peaking and the corresponding damping on the OJTF response.
When Peaking is selected in the results table, annotation is placed on the graph marking the location of the measurement.
The Peaking Frequency measurement requires FlexDCA version A.07.00 or later.
SCPI Command
:MEASure:RESPonse:PFRequency?
:MEASure:RMEMory:PFRequency?