Zero Frequency
Flex Apps:
FlexPLL
The Zero Frequency measurement indicates a single frequency in the JTF model where gain decreases. Similar to this is the Pole Frequency measurement that locates a single frequency in the JTF model where gain increases. A Type 2 PLL by definition has only one pole.
with Zero, Pole, and Gain Frequencies
SCPI Command
:MEASure:RESPonse:PLLModel:FZERo?
:MEASure:RMEMory:PLLModel:FZERo?