Peaking Magnitude
Flex Apps:
FlexPLL
Peaking Magnitude measures maximum peaking on the JTF response for a DUT that uses a 2nd Order PLL. The following figure shows a simplified JTF response with peaking and the corresponding damping on the OJTF response.
When Peaking is selected in the results table, annotation is placed on the graph marking the location of the measurement.
SCPI Command
:MEASure:RESPonse:PEAKing?
:MEASure:RMEMory:PEAKing?