IVxiMemacc::DestinationBigEndian
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Indicates whether the destination address space uses Big Endian or Little Endian byte order.
VB Prototype
Dim value As Boolean
value = object.DestinationBigEndian
object.DestinationBigEndian = value
C++ Prototype
HRESULT get_DestinationBigEndian(
VARIANT_BOOL* DestinationBigEndian
);
HRESULT put_DestinationBigEndian(
VARIANT_BOOL DestinationBigEndian
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, DestinationBigEndian, DestinationIncrement, SourceBigEndian, SourceIncrement, DestinationAccessPrivilege, SourceAccessPrivilege, LogicalAddress, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, In8, In16, In32, Out8, Out16, Out32, MoveIn8, MoveIn16, MoveIn32, MoveOut8, MoveOut16, MoveOut32, Move, IVxiMemacc Overview