IVxiMemacc::SourceAccessPrivilege

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Specifies the address modifier to be used in high-level access operations, such as InXX and MoveInXX, when reading from the source.

VB Prototype

Dim value As VXIMemoryAccessPrivilege
value = object.SourceAccessPrivilege

object.SourceAccessPrivilege = value

C++ Prototype

HRESULT get_SourceAccessPrivilege(
  VXIMemoryAccessPrivilege* SourceAccessPrivilege
);

HRESULT put_SourceAccessPrivilege(
  VXIMemoryAccessPrivilege SourceAccessPrivilege
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, DestinationBigEndian, DestinationIncrement, SourceBigEndian, SourceIncrement, DestinationAccessPrivilege, SourceAccessPrivilege, LogicalAddress, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, In8, In16, In32, Out8, Out16, Out32, MoveIn8, MoveIn16, MoveIn32, MoveOut8, MoveOut16, MoveOut32, Move, IVxiMemacc Overview