IVxiMemacc::SourceBigEndian
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Indicates whether the source address space uses Big Endian or Little Endian byte order.
VB Prototype
Dim value As Boolean
value = object.SourceBigEndian
object.SourceBigEndian = value
C++ Prototype
HRESULT get_SourceBigEndian(
VARIANT_BOOL* SourceBigEndian
);
HRESULT put_SourceBigEndian(
VARIANT_BOOL SourceBigEndian
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, DestinationBigEndian, DestinationIncrement, SourceBigEndian, SourceIncrement, DestinationAccessPrivilege, SourceAccessPrivilege, LogicalAddress, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, In8, In16, In32, Out8, Out16, Out32, MoveIn8, MoveIn16, MoveIn32, MoveOut8, MoveOut16, MoveOut32, Move, IVxiMemacc Overview