N9935A/36A/37A/38A
The adjustments for the spectrum analyzer functionality of the Fieldfox analyzer models listed above consist of five different adjustments:
IF Frequency Response
Depending on the firmware of the Fieldfox, TME will use one of two methods to run the spectrum analyzer adjustments.
For Fieldfox analyzers with firmware below A.09.00, TME will run the five adjustments in the traditional method, as separate adjustments. They should be run in the order shown below with minimal delay between adjustments. Temperature drift during these adjustments should be minimized. Delays of more than an hour between adjustments should be avoided as this may allow for excessive temperature drift.
Click on the links below to go to the individual adjustment topic pages:
For Fieldfox analyzers with firmware A.09.00 and above, TME will run the five spectrum analyzer adjustments as one "super" adjustment called the Spectrum Analyzer Adjustment. Click here to go the adjustment topic page.