This section lists the test equipment needed to run performance tests and adjustments. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. Refer to each individual test for specific setup configurations with required cables and adapters.
|
Test Equipment |
Recommended Model |
Alternate Model |
||
|
Analyzers |
||||
|
Spectrum analyzer for performance verification For these models :
|
N9030B with options:
|
N9030A
|
||
|
Spectrum analyzer for adjustments For these models:
|
N9030A Option 5xx Select any frequency option (503, 508, 513, 526, 544, 550) that has a maximum frequency greater than or equal to the maximum frequency of the unit under test. |
None |
||
|
Spectrum analyzer for performance verification tests For M9383A |
N9030B with options:
|
None |
||
|
Spectrum analyzer for adjustments For M9383A |
N9040B with options:
|
None |
||
|
Vector Signal Analysis Application Used with Wideband EVM Adjustment for the M9383A only. |
89600 VSA with licenses:
|
|
||
|
Sources |
||||
|
Function generator For M9381A |
33622A |
33612A |
||
|
Reference source For M9383A |
E8257D Options UNT, UNY,1EU |
E8267D Options UNT, [UNX or UNY] |
||
|
Power Meters and Sensors (See below for calibration service ordering guidelines.) |
||||
|
Power meter |
N1914A1
|
E4418A/B1
|
||
|
Power Sensor 1 For models:
|
For performance tests: N8482A |
E9304A-H20 |
||
|
For adjustments: E9304A-H20 |
E9304A-H18 |
|||
|
Power Sensor 1 For M9383A performance verification tests.
|
N8487A1
|
|
||
|
Power Sensor 1 For M9383A adjustments. |
N8488A |
None |
||
|
High-Power Power Sensor For M9383A Option 1EA or 1EB with performance verification tests.
|
E9304A-H191
|
E9300A-H251
|
||
|
Other Devices |
||||
|
High performance oscilloscope Used by the M9383A in the Pulse Accuracy Performance Test. |
DSOV334A1
|
DSAX92004A1 DSOX92004A1 MSOX92004A1 DSAV204A1, 2 DSOV204A1, 2 DSAZ204A1, 2 DSOZ204A1, 2
|
||
|
Phase noise measurement system For M9383A |
N5511A Options 540, CH21
|
E5505A Option 0011
|
||
|
100 MHz Reference1 |
M9300A1
|
N/A |
||
|
10 MHz Reference |
Microsemi 5071A |
House standard external reference |
||
|
Power splitter, 3.5 mm (f) |
11667B |
|||
|
Terminator, 50 W
|
909D |
N/A |
||
|
Fixed attenuator, 6 dB |
8493C Option 006 |
|
||
|
PXIe chassis |
M9018B |
M9018A |
||
|
PXIe system module
|
M9022A |
M9021A |
||
|
PXIe embedded controller
|
M9037A |
M9036A |
||
|
Cables |
||||
|
Cable to connect the oscilloscope to Trig 1 in the Pulse Accuracy Performance Test (M9383A) |
8121-2626
OR
8121-2627 AND 1250-1237 |
|
||
|
3.5 mm (m) to 3.5 mm (m)
|
11500E |
8120-4921 |
||
|
3.5 mm (m) to 3.5 mm (m)
|
8121-1221 |
|
||
|
BNC (m) to SMB (f) |
8121-2063 |
|||
|
BNC (m) to BNC (m) |
8120-2582 |
10503A |
||
|
SMB (f) to SMB (f) |
8121-2175 |
|||
|
Adapters |
||||
|
Type-N (f) to 3.5 mm (m) |
1250-1750 |
|||
|
3.5 mm (f) to 2.4 mm (f) |
11901B |
|||
|
BNC Tee |
1250-0781 |
|||
|
Type-N (f) to SMB (f) |
Any |
Crestwood Technology Group P/N 510776701 |
||
To use the PXA N9030A with N9063A analog demodulation measurement application functionality above 3.5 GHz, the N9030A must be upgraded with one of the following upgrade options: MTU or TES. After either upgrade, the N9030A must be re-calibrated for analog demodulation specifications above 3.5 GHz to be valid.
Choose from one of the following options:
Option MTU — Multi-Touch User Interface
For analog demodulation specifications above 3.5 GHz to be valid, Option MTU can only be installed on N9030A instruments with serial number prefix greater than or equal to MY/SG/US5449.
Option TES — TOI Enhanced Specifications
Option TES is a Keysight-only internal option. Keysight service centers need to contact the CSG support node to obtain an internal license key for this option.
USB power sensors require a power meter with USB ports. The table below shows the various options that will provide USB ports on the TME recommended N1914A power meter.
|
N1914A Orderable Options |
Description |
FW responds as option1 |
|
|
201 |
Ordered from the factory with new N1914A |
Dual channel average power meter with VGA, trigger in/out, 1 front and 1 rear USB port |
008, 010, 012 |
|
The following options are ordered as upgrades to an existing N1914A power meter. |
|||
|
106 |
This is the recommended option. |
Dual channel average power meter with 1 front and 1 rear USB port |
008 |
|
103 |
alternate |
Dual channel average power meter, battery, 2 rear USB ports |
001, 009 |
|
105 |
alternate |
Dual channel average power meter with VGA, battery, 1 front and 1 rear USB port |
008, 010 |
|
108 |
alternate |
Parallel rear-panel sensor input connectors, front-panel reference calibrator connector, 2 rear USB ports |
002, 009 |
|
109 |
alternate |
Parallel rear-panel sensor input connectors, rear-panel reference calibrator connector, 2 rear USB ports |
003, 009 |
|
111 |
alternate |
Dual channel average power meter, battery, 1 front and 1 rear USB port |
001, 008 |
|
167 |
alternate |
Dual channel average power meter, external trigger in/out, 1 front and 1 rear USB port |
008, 012 |
|
Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.
The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.
Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can be imported into TME thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor and not for new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|