The performance verification tests are designed to provide the highest level of confidence that the instrument being tested conforms to the published, factory-set specifications. The tests are designed to test an instrument operating within the temperature range defined by the instrument specifications. The recommended calibration cycle is every 12 months.
|
|
|
Each test will check at the beginning and at the end of the test that modules are not exceeding the maximum module temperature specification for that test. A warning will be given to the user if a module temperature is exceeded. Refer to the Recommended Practices for Module/Chassis Temperature Control for more information.
Performance tests are listed in the order that they should be performed. Select from the links below for your model number.