Keysight 89600 VSA .NET API
ConstellationState Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace : ConstellationState Class

Glossary Item Box

The following tables list the members exposed by ConstellationState.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyImaginaryGets or sets the imaginary (or "Q") value for the constellation state location.  18.00
Public PropertyIndexGets the zero-based state index of this constellation state location within the constellation.  18.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMagnitudeGets or sets the magnitude value for the constellation state location.  18.00
Public PropertyPhaseGets or sets the phase value for the constellation state location in degrees.  18.00
Public PropertyRealGets or sets the real (or "I") value for the constellation state location.  18.00
Public PropertySymbolGets or sets the symbol data represented by this constellation state location.  18.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also