Keysight 89600 VSA .NET API
DigitalChannel Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : DigitalChannel Class

Glossary Item Box

The following tables list the members exposed by DigitalChannel.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAcquisitionIndexGets the zero based index of which acquisition this channel will be a part of when sequential input channels are being used where the same physical channel can be re-used for sequential acquisitions. This property will return 0 when part of the first acquisition in sequential inputs or when sequential inputs are not being used. (Inherited from Agilent.SA.Vsa.InputChannel)25.00
Public PropertyDataBusPart1Gets or sets the data bus name used for part 1 of the channel data (e.g. I or Q).  —
Public PropertyDataBusPart2Gets or sets the data bus name used for part 2 of the channel data (e.g. I or Q).  —
Public PropertyDataModuleGets or sets the name of the logic analyzer module from which data will be taken.  —
Public PropertyDataScalePart1Gets or sets the data scaling factor for part 1 of the channel data.  —
Public PropertyDataScalePart2Gets or sets the data scaling factor for part 2 of the channel data.  —
Public PropertyDataSignGets or sets how signed numbers are represented.  —
Public PropertyDataToolGets or sets the name of the logic analyzer tool from which data will be taken.  —
Public PropertyDisplayNameGets the display name for the input channel. (Inherited from Agilent.SA.Vsa.InputChannel)—
Public PropertyIdGets the unique identifier for the physical input channel. (Inherited from Agilent.SA.Vsa.InputChannel)—
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetDataBusNamesReturns a list of data bus names at the output of the given module or tool.  —
Public MethodGetDataToolNamesReturns a list of tool names available at the output of a given module.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also