Keysight 89600 VSA .NET API
SequencedPlaybackMode Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementCollection Class : SequencedPlaybackMode Property


Glossary Item Box

Gets or sets a value indicating how sequenced recording playback is coordinated between measurements.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SequencedPlaybackMode As SequencedPlaybackMode
C# 
public virtual SequencedPlaybackMode SequencedPlaybackMode {get; set;}
C++/CLI 
public:
virtual property SequencedPlaybackMode SequencedPlaybackMode {
   SequencedPlaybackMode get();
   void set (    SequencedPlaybackMode value);
}

Property Value

The default value is SequencedPlaybackMode.Independent

Remarks

This property adjusts the measurement sequencing order for measurements using recording playback (Input.DataFrom). This property is only used when Acquisition is set to AcquisitionType.Sequenced and at least two Measurement have Input.DataFrom set to DataSource.Recording. When SequencedPlaybackMode.TimeTracking is selected, sequencing will prioritize recording playback measurements with Recording.PlayPosition closest to Recording.PlayStart. This allows measurements with different Time.Length to loosely track each other in time.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40

See Also