Keysight 89600 VSA .NET API
Operation Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : Operation Class

Glossary Item Box

The following tables list the members exposed by Operation.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyCancellationSupportedGets a value indicating whether the operation can be canceled".  —
Public PropertyExceptionGets the exception (if any) that caused the operation to fail (State is OperationState.Failed).  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMessagesGets the messages that have been logged during the operation.  —
Public PropertyMessagesSupportedGets a value indicating whether the operation reports progress messages.  —
Public PropertyNameGets the display name of the operation.  —
Public PropertyProgressGets the progress of the operation as a value between 0.0 and 100.0.  —
Public PropertyProgressSupportedGets a value indicating whether the operation will report Progress.  —
Public PropertyStateGets the current state of the operation.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodRequestCancellationRequests cancellation of the operation.  —
Public MethodWaitForCompletionWaits for the operation to complete and times out if not completed within timeoutMS.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also