| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property CellBeamSeparationMethod As CellBeamSeparationMethod | |
| C# | |
|---|---|
public virtual CellBeamSeparationMethod CellBeamSeparationMethod {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property CellBeamSeparationMethod CellBeamSeparationMethod { CellBeamSeparationMethod get(); void set ( CellBeamSeparationMethod value); } | |
Property Value
The default value is CellBeamSeparationMethod.PSS.see the definition of CellBeamSeparationMethod, when PSS or CRS method is selected, customer needs to tell the interference cell IDInterferenceCellId when spatial filter is selected, customer needs to tell the measured cell beam direction, the horizontal angleCellBeamDirectionPhi and the vertical angleCellBeamDirectionTheta.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20