Keysight 89600 VSA .NET API
UplinkUser Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : UplinkUser Class

Glossary Item Box

The following tables list the members exposed by UplinkUser.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyCellIdGets or sets the Cell ID for the UL user  —
Public PropertyIncludeGets or sets a value indicating whether the UL user is included in EVM calculations and shown in traces.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsGroupHoppingEnabledGets or sets a value indicating whether Group Hopping is enabled for the UL user.  —
Public PropertyIsSequenceHoppingEnabledGets or sets a value indicating whether Sequence Hopping is enabled for the UL user.  —
Public PropertyNameGets or sets the name for the UL user.  —
Public PropertyPrachGets the PRACH channel of the UL user.  —
Public PropertyPucchGets the PUCCH channel of the UL user.  —
Public PropertyPuschGets the PUSCH channel of the UL user.  —
Public PropertyRntiGets or sets the RNTI for the UL user  —
Public PropertySrsGets the SRS channel of the UL user.  —
Public PropertySystemFrameNumberGets or sets the System frame number for the UL user  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also