Keysight 89600 VSA .NET API
ThreeSectorAntennaPattern Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : ThreeSectorAntennaPattern Class

Glossary Item Box

The following tables list the members exposed by ThreeSectorAntennaPattern.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyDowntiltAngleGets or sets the downtilt angle of the three sector antenna pattern.  27.00
Public PropertyFrontToBackRatioGets or sets the front to back ratio of the three sector antenna pattern.  27.00
Public PropertyHorizontalHalfPowerBeamwidthGets or sets the horizontal half power beam width of the three sector antenna pattern.  27.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyScanAngleGets or sets the scan angle of the three sector antenna pattern.  27.00
Public PropertySideLobeSuppressionGets or sets the side lobe suppression of the three sector antenna pattern.  27.00
Public PropertyVerticalHalfPowerBeamwidthGets or sets the vertical half power beam width of the three sector antenna pattern.  27.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also