Keysight 89600 VSA .NET API
CarrierConfiguration Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : CarrierConfiguration Class

Glossary Item Box

The following tables list the members exposed by CarrierConfiguration.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyCellIdGets or sets the physical layer Cell ID.  27.40
Public PropertyEnabledGets or sets a value indicating whether the component carrier is enabled or not.  —
Public PropertyIntegrationBandwidthGets or sets the integration bandwidth of the component carrier in Hz.  —
Public PropertyIntegrationBandwidthAutoGets or sets a value indicating whether the integration bandwidth of the component carrier is automatically configured.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMaxTransmissionBandwidthGets or sets the transmission bandwidth used by the CarrierConfiguration.  —
Public PropertyNumerologyGets or sets the numerology used by the CarrierConfiguration.  —
Public PropertyRelativeFrequencyGets or sets the frequency of the component carrier relative to the StandardSpecificConfiguration.CarrierReferenceFrequency.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also