Keysight 89600 VSA .NET API
HopAnalysis Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : HopAnalysis Class

Glossary Item Box

The following tables list the members exposed by HopAnalysis.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyEnabledGets or sets a value indicating whether hop analysis is enabled.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsMaxDwellTimeLimitEnabledGets or sets a value indicating whether the maximum dwell time limit is enabled.  —
Public PropertyIsMinDwellTimeLimitEnabledGets or sets a value indicating whether the minimum dwell time limit is enabled.  —
Public PropertyMaxDwellTimeGets or sets a value indicating the maximum dwell time (seconds) that will be detected.  —
Public PropertyMinDwellTimeGets or sets a value indicating the minimum dwell time (seconds) that will be detected.  —
Public PropertyPulseFrequencyPhaseHopDwellWidthGets or sets the center portion (%) of the dwell used for frequency and phase calculations.  —
Public PropertySettlingToleranceGets or sets the allowed frequency (Hertz) deviation for hop settling detection.  —
Public PropertyStateDetectionModeGets or sets a value indicating how state analysis is done in the measurement.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetStatesGets the hop analysis states.  —
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetStatesSets the hop analysis states.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also