Keysight 89600 VSA .NET API
InterferingSignal Class Members
See Also  Properties  Methods  Events
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace : InterferingSignal Class

Glossary Item Box

The following tables list the members exposed by InterferingSignal.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyEnabledGets or sets a value indicating whether the interfering signal exists.  —
Public PropertyFrequencyOffsetFromEdgeGets or sets the offset frequency from the edge of sub block. Units are Hz.  —
Public PropertyIsAtInnerOffsetGets or sets a value indicating whether this interfering signal is at an inner offset area or not  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyOffsetSideGets or sets which side of interfering signal is present.  —
Public PropertyReferenceSubblock1Gets or sets the ID of subblock1 this interfering signal is referencing.  —
Public PropertyReferenceSubblock2Gets or sets the ID of subblock2 this interfering signal is referencing.  —
Public PropertyReferenceSubblock2EnabledGets or sets a value indicating whether the ReferenceSubblock2 is used as a reference or not.  —
Public PropertySpanGets or sets the span of the interfering signal. Units are Hz.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also