The following tables list the members exposed by QuickSetupCollection.
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | Count | Gets the number of items in the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<QuickSetup>) | — |
![]() | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | Item | Overloaded. Gets the indicated QuickSetup from the collection by string name. | 26.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | Contains | Gets a value indicating whether a QuickSetup was found in the collection matching the provided name. | 26.00 |
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetEnumerator | Gets an enumerator for the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<QuickSetup>) | — |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | IndexOf | Overloaded. Gets the index location of the specified item within the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<QuickSetup>) | — |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | CollectionChanged | Occurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<QuickSetup>) | — |
![]() | PropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | PropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemoteCollectionChanged | Occurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<QuickSetup>) | 14.00 |
![]() | RemotePropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | 14.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||