Select Subcarrier Region (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
specifies which subcarriers are analyzed and included in the measurement data results when the VSA is set to Uniform Data Analysis mode.
: Shows data results for the specified subset of subcarriers defined by the Subcarrier Offset and Subcarrier Interval parameters.
: Shows all data results for all subcarriers (excluding subcarrier 0).
The parameter on the tab must be cleared for the Select Subcarrier Region check box to be displayed.
See Also