Preamble Index (802.16 OFDMA)
: 0 (See OFDMA Standard Presets Table.)
(applies to only)
specifies the preamble sequence for the downlink subframe.
To correctly demodulate the pilots and synchronize to the downlink subframe, the must be associated with the proper IDCell and Segment values. Override Preamble Definition determines what and values are used by the VSA.
See Also