Uplink Subframe (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
Subframe Type sets the VSA to Uplink analysis mode. The VSA will demodulate and analyze the uplink subframe within the current OFDMA analysis frame (applies to both Uniform Zone analysis mode and Data Burst Analysis mode).
1) When is selected, all uplink unique demodulation properties will be made active and all Downlink demodulation properties will be made inactive (greyed out).
2) To measure the Downlink subframe, set the VSA to Downlink Subframe Type.
See Also