Enable additional demodulator settings (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
enables the additional parameters on the tab as well as the Override Measurement Region settings on the tab.
Additional Advanced tab Parameters:
- Compensation Parameters:
- Data Tone Modulation parameters:
- Equalizer Training Parameters:
- Pilot Tracking Parameters:
Additional Time tab parameters
See Also