Unknown Pilot Power Boost Level (Custom OFDM)
: See Preset to Standard
The parameter specifies the boost power level for each Unknown Pilot subcarrier. A value of 1 equals "no boosting" and a value of 2 equals "6.02dB" of boosting. The boosting level is unitless and relative to the reference power level.
| Unknown Pilot Power Boost Level | Boosting Level |
|---|---|
| 1 | No boosting |
| 2 | 6.02 dB |
The Unknown Pilot subcarriers are Resource type 2, see Resource Map.
See Also