Power Boost Level Per User (Custom OFDM)
This property is only valid when Resource Interface = Type1.
: See Preset to Standard
The parameter specifies the boost power level for each user. A value of 1 equals "no boosting" and a value of 2 equals "6.02dB" of boosting. The boosting level is unitless and relative to the reference power level.
If the array is too short, any values past the end are assumed to be 1.
See Also
QAM Identifier Power Boost Levels