QAM Identifier Power Boost Levels (Custom OFDM)
: See Preset to Standard
The parameter specifies the boost power level for each QAM Identifier. This is an array with one value for each Identifier in the QAM Identifiers The QAM Identifiers parameter is specified in the Format tab > QAM Idenifiers text box (Custom OFDM Demod Properties dialog box). array. A value of 1 equals "no boosting" and a value of 2 equals "6.02dB" of boosting. The boosting level is unitless and relative to the reference power level (see Power Reference Level).
| QAM Quadrature Amplitude Modulation Identifier | Boosting Level |
|---|---|
| 1 | No boosting |
| 2 | 6.02 dB |
When the QAM Identifier Power Boost Levels array is less than the number of QAM Identifiers array, a Boost level is assumed to be 1 for any additional QAM Identifiers.
See Also