Signal is Bursted (Custom OFDM)

Analysis > Custom OFDM Demod Properties > Format tab

This parameter is shown in the Frame Definition tab and the Format tab. When Frame Definition > Apply is clicked, the value in the Frame Definition tab is applied to the Format tab (and the signal).

 Default: See Preset to Standard

The Signal is Bursted parameter specifies the signal transmission type: Bursted (Pulsed) or Continuous.

Selected: Bursted (Pulsed)
Cleared: Continuous

See Also

Custom OFDM Demod Properties