Average Tab (MeasSetup)
The tab sets averaging parameters and turns averaging on or off.
-
Average Type selects an averaging function.
-
Count specifies the number of averages to perform.
-
Repeat Average is valid only for linear average types and causes the VSA to continue instead of stopping after completing the average.
-
Fast Average is used to increase measurement speed for some configurations. When Fast Average is enabled, the VSA updates the display only after accumulating the number of averages specified by .
-
Update Rate is used with (described above).
See Also
Averaging with Digital Demod, WCDMA, and cdma2000 demodulation