X-Axis Popup Menu
Right-clicking below the trace grid opens the X-axis popup menu, which changes the following frequently used parameters.
sets X-axis scaling so the entire X-axis is shown (same as ).
opens the X Scale tab, which changes X-axis scaling and other X-axis parameters.
displays the Format tab (same as clicking from the main menu), selects trace coordinates.
displays the Coupling tab (same as clicking from the main menu), selects coupling with overlaid traces.
displays the Average tab (same as clicking from the main menu), selects trace averaging.
opens the Frequency tab, which sets frequency parameters.
opens the ResBW tab, which sets resolution bandwidth parameters.
opens the Time tab, which sets parameters for time-domain and time-gating analysis.
opens the Trigger tab, which sets trigger parameters.
opens the Playback Trigger tab which sets trigger parameters for recordings.
selects the measurement to which this trace belongs.