Time Tab (Analysis)

The Time tab gives access to time-domain and time gating parameters.

The time-domain parameters are:

Time Gate

The Time Gating Parameters are:

Time tab parameters, except overlap settings, are available only for Analog Demod or Vector measurements.

To specify time record lengths in other measurement types, use the Time tab in the Demod Properties dialog.

See Also

Overlap Processing

Main Time (Trace Data)

Gate Time (Trace Data)

About Time Gating