Saving a Recording
Follow these steps to save a recording:
-
Click
-
In the dialog box, select a file format and type the filename. A recording can be saved using any of the file formats documented under Saving and Recalling Recordings.
-
Click .
-
Select options from the Save Options dialog box (except for SDF file format).
Signal Recordings for Source Playback
If you need this recording for source signal playback, you need to save the file as a MATLAB "*.mat" formatted file and select the "Save header with data" Save Option ().
Saving a Segmented Recording
When saving a segmented recording Between playback start/stop times, the start/stop times will be expanded to include a whole number of segments (e.g. if the playback start time falls in the middle of a segment, the start time of the saved recording will be the beginning of that segment).
See Also