Normalize IQ Traces (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Advanced tab

Default:Select (See MB-OFDM Standard Setups/Presets Table.)

Normalize IQ Traces has the effect of setting the outermost state of the ideal constellation diagram to a magnitude of one (1), thus IQ Meas and IQ Ref trace data results are normalized.

See Normalize IQ Traces (Digital Demodulation) for more information.

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Advanced Tab (MB-OFDM Demod Properties)