IQ Ref (MB-OFDM)
Menu Path:
The composite is a subcarrier-domain trace that shows the ideal IQ symbol values of the subcarriers across the selected symbol-times (bursts) for all occupied bands. The symbol-times of interest are selected using Result Length, Measurement Offset, and Measurement Interval (the results of these settings appear as TimeLen on the trace). To learn more, see Lengths, Intervals, and Offsets. The IQ Meas displays a setup example. For trace identification, the pilot and guard symbols are colored differently than the data symbols.
See Also
Available Trace Data (MB-OFDM)