Phase Track Average Length (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Advanced tab

Default: 4 symbol-times (TFC 1 to 4) | 12 symbol-times (TFC 5 to 7) (See MB-OFDM Standard Setups/Presets Table.)

Range: 1 to 1000 symbol-times

Phase Track Average Length sets the length in symbol-times of the average that is used in tracking phase changes during demodulation. A lower value allows changes in the phase of the signal (as in phase noise) to be tracked more quickly, while a longer range allows the phase reference for the demodulation to be better smoothed and not respond so quickly to phase changes in the signal.

Phase Track Average Length is inactive when Auto CPE Filter Length is selected.

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Auto CPE Filter Length (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Advanced Tab (MB-OFDM Demod Properties)