Time Tab (Pulse)

Menu Path: Analysis > Pulse Properties > Time

The Time tab lets you set time-domain parameters for pulse measurements, such as Acquisition Length and Sample Rate. It also lets you set a count for segmented captures, define which pulse is the starting pulse in the measurement, and the number of pulses to include. Furthermore, you can specify a portion of the pulse, instead of the entire pulse, to show on traces.

See Also

Acquisition Length

Sample Rate

Extra Acquisition

Segmented Capture

Selected Pulses

Highlight Selected Pulses

Include Extra Data Before and After