Both (RFID)
: Cleared (See RFID Standard Setups/Presets Table)
To avoid confusion, particularly when the VSA has averaging enabled, the specifies which type of measurement is desired: , , or .
When mode is selected, all results are computed. Averaging is rejected if no burst is found or if CW power-on and CW power-off are not found in the data.
See Also