Auto-Detect Midamble (TD-SCDMA)
The button will cause the Basic Midamble Code ID to be detected from the signal and then both and the Code IDs are set to this value. It is recommended that the Force Code Group parameter be set to .
Automatic midamble detection is only functional when is selected for Subframe Synchronization ( tab). When is not selected, is not available.
See Also