Downlink Pilot (TD-SCDMA)
0 (See TD-SCDMA Standard Setups/Presets Table.)
: 0 to 31
specifies the Downlink Pilot Synchronization ID sequence. These codes are used for DL Down Link (forward link: from base station to cell phone) synchronization and cell initial search (see TD-SCDMA - Code/ID Allocation Overview).
See Also
TD-SCDMA Overview - Code Allocation