GPS Commands


In this topic:

Note: Some commands are hardware and option dependent.

See Also

- Commands that are Common to All Modes

- Correction Methods Explained

- New Programming Commands

- Status Registers

 

GPS

Sets the minimum satellite power, before computation

:SYSTem:GPS:AVERage:MINP

Enables/disables the satellite average settings

:SYSTem:GPS:AVERage[:STATe]

Sets the number of satellites to be viewed

:SYSTem:GPS:AVERage:TOPN

Query satellite carrier to noise

:SYSTem:GPS:CNOise?

Returns GPS data

:SYSTem:GPS:DATA?

Returns the last locked GPS data

:SYSTem:GPS:DATA:LAST?

Set and qjuery the coordinates (i.e., lat. & long.)

:SYSTem:GPS:DISPlay:COORdinate:FORMat

Set and query the elevation units

:SYSTem:GPS:DISPlay:DISTance:UNIT

Set and query the status line display state

:SYSTem:GPS:DISPlay:STATe

Set and query the type of satellite being measured

:SYSTem:GPS:GNSS

Returns the GPS lock state

:SYSTem:GPS:LSTate?

et the GNSS fast update rates

Set and query the GPS state

:SYSTem:GPS[:STATe]

Set and query the GPS clock sync state

:SYSTem:GPS:SYNChronize

 


Last Modified:

09dec2019

Added new topic/commands