(Read-Only) Returns the current USB/LAN sensor's model number string and serial number string values. See also, INP:TYP, INP:LAN:ADDR, INP:LAN:ID:SNUM, INP:LAN:ID:TYP, INP:LAN:ID:NAME, and DISP:MOD:STAT. Learn more, the FieldFox Supplemental Help. |
|
Relevant Modes |
Frequency Offset mode (Option 208), Power Sensor (USB) Mode - Option 302, Power Meter mode (Option 310), and Pulse Measurements mode (Option 330) |
Parameters |
|
Examples |
DISP:MOD:DATA? |
Return Type |
Comma-separated string |
Default |
Not Applicable |
Last modified:
01june2019 |
New command (11.26) |